This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510 always in sealed mode

Other Parts Discussed in Thread: BQ27510

Hi,

I have a problem with a fuel gauge which is always in sealed mode.

I have 2 board :

A : my electronics card with bq27510 and battery ref BAT

B : the bq27510 evaluation board with the same battery

I connect this card to BQ evaluation software with EV2300 module

When I download the bq27510default dataflash file (BqEasy step 1.B) to the boards A and B, it's work. But after the board B is in sealed mode and board A in full access mode.

After, I send unsealed and full access key to the board B

Then I send (with I2C pro) the full reset command to the boards A and B. After that, board B is in sealed mode and board A in full access mode.

After, I send unsealed and full access key to the board B

If I disconnect the battery from boards A and B, when I reconnect it, board B is in sealed mode and board A in full access mode.

 

I think that there is a problem on board B but I don't understand wher it is.

May I have some help ?