Hello guys,
Working on BQ24773 charger IC. Couple of questions are waving in mind. Please help.
Pre-info:
- I am using PIC32 controller to communicate with BQ24773 IC which is connected to battery through fuel gauge IC.
Questions:
- How BQ IC functions?
- Which are the pins used for charging battery?
- Does BQ IC sense battery voltage and current automatically? OR do we need to configure any pins to sense parameters?
- How much voltage and current value to be set for battery charging? (Using two batteries: 1) 7.4V 3000mAh Lipo rechargeable 2) 3.7V 2200mAh rechargeable )
- Should charging be done through register configuration only?
Request:
- If you any reference documents please share with me.
- If you any reference firmware code, please share with me.
Looking forward to your support.
-Harshit