This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: using UCC28950 for Sepic function

Part Number: UCC28950


Hi! TI Supports,

I would confirm whether We can use UCC28950 to build a DC/DC converter to convert 120V to 240V DC into 200V/400V (2A/1A). The application is for Solar panel  DC/DC application. Yes, I would like to use the ZVS, ZCS topology. Please double confirm it.

Thank you very much!

Johnson