Other Parts Discussed in Thread: TPS54361, , LM5175, LMR14050-Q1
Team,
Our customer is now working on TPS54361 for the spec : Vin=30-20V, Vo=24.5V, Io=10mA - 2A
However, TPS54361 DS describes;
"To reduce the losses of the small low-side MOSFET at high output voltages, the small low-side MOSFET disables at 24-V output and re-enables when the output
reaches 21.5 V."
So, when Vin is close to Vo, TPS54361 cannot work with high duty.
On the other hand, LMR14030 DS has no description about the similar contents of TPS54361.
Can LMR14030 work with high duty even when Vo > 24V ?
よろしくお願いします。
Thanks and Regards,
Metropolitan (Tokyo) Area FAE Kenji Ninagawa