Dear pros of texas instruments,
I am researching on a suitable buck boost converter that is able to power any smartphone of up to 2A and is also flexible enough to change to power an ac load (Say maybe a light bulb).
Through my research I found a simple buck boost converter schematic that made use of the LTC3440 chip.
(http://www.circuitstoday.com/buck-boost-converter-circuit)
However, it only has a maximum output of 600mA which is insufficient to power up any smartphone of today in 2017.
What ic chip/components should I use to further increase the output current if i were to retain the same design?
Hope to receive any input from the committee here.
Regards
John