This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM338: LM338K

Part Number: LM338
Other Parts Discussed in Thread: TPS759

Hello,

Would you please tell me if there is a components that pin to pin compatible with the LM338K and that provide more than 5A in output?

Best regards,

  • Hi Said,

    The only linear regulator we have that is rated for greater than 5A in a single package is TPS759; however, it is not pin to pin compatible. Typically for higher current applications two or more LDOs are paralleled. The following TI-Design gives an example of how this can be done www.ti.com/.../tidu421.pdf

    Very Respectfully,
    Ryan
  • Hi Ryan,

    Thank you for your quick reply.

    We have an equipement wich feeds the motor of a door, the peak current exceeds 15A.

    In the equipement there are 3 LM338K in parallel.

    The problem is that after a few years the component (LM338K) breaks down.

    That why i think if there is an equivalent component that provide more than 5A can resolve the problem.