This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TpS1H100-Q1: about Switching Characteristics

Guru 20090 points
Part Number: TPS1H100-Q1

Hello,

In the datasheet Switching Charateristics, the condition is RL=10ohm.
Are there other load specification ? (for example, 5ohm or 15ohm).

Also, could you please let me know the load condition of Figure 17 and Figure 18? Is this data RL=10ohm?

Best Regards,
Ryuji 



  • Hello Ryuji,

    Figure 17 and 18 use RL = 10ohm. This is specified in section 7.7 "Switching Characteristics" of the datasheet.
    The plot's test conditions for each specification are shown in the corresponding "Test Conditions" column of the "Electrical Characteristics" (section 7.6) and "Switching Characteristics" (section 7.7) tables

    Best,
    Nick