Other Parts Discussed in Thread: LM5026, LM5025, TIDA-00181, LM25037
Hi Team,
We got a request from customer as below, could you kindly help on it, please?
Pls see below for my design requirements:
- Vin: 25-50V
- Vout: (all rails need to be independent of each other)
- - Vo1: 5V (tol=1%), Io=12A, Iocp=20A (hold on 50ms before hiccup launches)
- - Vo2(3): +/-15V (tol=3%), Io=6.5A, Iocp=10A (hold on 350ms before hiccup launches)
- - Vo4(5): +/-24V (tol=3%), Io=3A, Iocp=10A (hold on 8s before hiccup launches)
- -Vdd (for UCC2897A): 12~15V, Io=0.3A
OCP: shall be hiccup mode whenever fault is removed
OVP: latch mode
Transient: 5% in all conditions
Ripple: <1.25% (Vpp)
Isolation (hipot) test voltage
- P-S 2000V 1min
- S-CGND 700V 1min
Ta: -45~90 oC
Could you pls review my key points above and recommend some applications? Can UCC2897A fulfill this application?
thanks!
Bell