We have a Half-Bridge isolated DC/DC converter based on UC28025 in production, that often has failed with high primary current (current sense resistor blown up).
The design of the circuit is based on symmetry between high and low side switching (midpoint of trafo is decoupled with capacitors that can not withstand the total supply voltage which is 400V)
Looking into the behaviour of the circuit under start-up, the high-side gate drive output (OUTA/pin11) is missing quite a lot of pulses (app. 10), and this also sometimes happens after the starrt-up period.
From the Functional Block Diagram, this should not be possible, as the output is chosen by a Toggle Flip-Flop sequentially, -A-B-A-B...
All signals on the other pins on the IC look correct.
What can our problem be?