This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020-Q1: average current

Part Number: TPS63020-Q1


Hi

I have a simple question.

This device has a average (inductor) current limit in the high side (buck)switch.

So that , we can estimate a current limit as following at each mode,

 at Boost : Iave = Eff * Isw * Vin/Vout

 at Buck : Iave = Iout

Is my understanding correct?

Regards,

Koji Hamamoto

  • The average current is detected in the switches and limited in the control circuit. In boost mode this current limit defines the maximum average input current and in buck mode this current limit defines the maximum average output current for the converter.