This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2846: Gate Drive Turn on Delay is extending dead time

Part Number: UC2846


Can someone explain to me why there is a 500nS delay between the sync pulse going low and the Gate drive going high? See plot below.   I need a shorter dead-time and the propagation delay seems to be the dominant factor.  The current oscillator set up is as follows:

Ct= 470pF

Rt=7k ohm

The oscillator calculation says I should be getting a 68nS dead time, of which I'm getting 240nS dead time pulse, which does not include this turn on delay.  Any help to minimize this turn on propagation delay would be appreciated.

The IC states a 500KHz operation, could I be to close to that, or off in the weeds where none of the equations work?

The oscillator in plot below is running at 450KHz, and my supply is running at 225KHz, is the 500KHz max oscillator frequency or supply frequency?

IF this part doesn't like the higher frequencies, Is there a device that could be more suitable for higher frequency operation that is pin compatible?

Thanks in advanced for you help

  • Hi Mark,

    Sorry for the delay in replying to you. The plots are not visible on the post can you try posting them again?

    Thanks

    Peter
  • Hello Mark,

    With the values of CT and RT that you chose, the expected oscillator frequency is 668kHz according to equation 3 in the datasheet.

    And this should give an expected dead time of 73nS according to equation 2.

    You should see a 73nS delay on one of the output drives. Is it possible there is some measurement error in your test?

    The plot was not attached so I cannot view your waveforms

    Regards

    John