Hi all
Would you mind if we ask TPS61029?
In case of exceeding switch currrent, which does the device operate as follows?
1. The device stops switching operation.
2. The device limits the current between 1.5A(Min) and 2.1A(Max).
If above content is "2", what will be the device stopping condition? Enable and Thermal shutdown?
We could not understand on the datasheet correctly.
Kind regards,
Hirotaka Matsumoto