This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Why bq2084 MaxError become 25% in the host system?

Hi All,

 

1) I have a bq284 (V1.33) battery pack return from host system, MaxError is 25%, but the MaxError is 2% when ship out. Could you please provide some possible for this phenomenon?

2) The bq2084 datasheet mention that "voltage-based corrections are applied to the coulomb counter, MaxError() is set to 25%.", how to understand this point?

 

Thanks & regards,

  • The are a couple of ways that MaxError could be set to 25%. 

    First, MaxError increments 1% for every 4 cycle counts without a learning cycle.  A learning cycle involves discharging the battery down to 7% RSOC. The gauge makes an FCC correction here and will set the MaxError back to 2%.  If your application does not allow the battery to discharge down to 7% every once in awhile, then MaxError will increase.

    The second way MaxError can be set to 25% is on a voltage correction, as you stated in point 2).  After a reset or loss of power, the gauge, upon power up, will set the RSOC to 25%, 50%, or 75%, depending on the Voltage. The VOC25, VOC50, and VOC75 thresholds determine what voltage corresponds to each percentage. After a learning cycle (discharging down to 7%), the gauge will learn a new FCC and the MaxError will drop to 2%.

  • Dear Chase,

     

    Thanks for your quickly respond.

     

    Thanks & regards,

    Suren

  • I happened to see a similar case recently. So to add to Chase's reply, there is an additional mechanism to set MaxError. It's in Gauge Configuration (0x29) VCOR bit. If this is enabled, a "midrange capacity correction" can occur when condition permits. See "Midrange Capacity Corrections" section in the datasheet.

  • Hi SW,

     

    Thank you share the information to us.

    If VCOR is enabled and keep the pack in the storehouse (The loss of power only self-discharge), whether the pack will be do voltage correction and midrange capacity correction?

     

    Thanks & regards,

  • I think it will.