This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2665: Supporting measurement

Part Number: LM2665


Hi,

Can I check for some supporting measurement data on:

 

(1)   Power efficiency at 1.4V, 2~4mA condition. According to datasheet, it should be 90% min, with typical 94%.

 

 

(2)   Shutdown current

 

Typ 1uA, what is the maximum and minimum value?

 

 

Thanks and best regards