Hi,
Now I'm evaluating bq25703A EVM and check the behavior at transition from supplement mode to battery operation. Then I confirmed the unexpected low pulse current duration after moving to battery operation as attached. Can you give your opinion why such behavior is happened?
Here is test set up.
- Input source : DC power supply 9.0V
- Battery input : DC power supply 8.4V, only source capability but battery current is only discharge at this condition
- Input current limit setting : 500mA
- System load : Electrical load 1000mA, that means 500mA discharge at supplement mode
Best Regards,
Satoshi / Japan Disty