This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: Connect with TPS61200

Part Number: BQ25504
Other Parts Discussed in Thread: TPS61200,

Hello, I am designing a circuit to charge a set of 3.7 V cells using a solar panel. For this I will use the BQ25504. Also I want to use the cells to power a 5V sensor, for this I want to use the TPS61200. So you would have the TPS connected to the cells and the BQ25504. Can this be a problem? How could I prevent the TPS from taking power from the BQ25504 and not from the cells? Thank you Schematic attachment.
Hello, I am designing a circuit to charge a set of 3.7 V cells using a solar panel. For this I will use the BQ25504. Also I want to use the cells to power a 5V sensor, for this I want to use the TPS61200. So you would have the TPS connected to the cells and the BQ25504. Can this be a problem? How could I prevent the TPS from taking power from the BQ25504 and not from the cells? Thanks
Schematic attachment.