Hi,
A bit of basic information about the set-up:
- Standalone application.
- 18650 battery (discharging @1.3 constant current).
- No Input Source.
The discharge of the battery looks all good until you reach the 2.5ish volts. I was expecting the FET to switch OFF completely and cut off the current to Vsys. However, I find that the Vsys and Isys are switching at 20Hz approx.
- Vsys between 2.45V and 0V (pulse width 1ms)
- Isys between +40mA and -40mA
Vsys progressively gets lower so does the Isys. However, at the beginning of the switching I saw spikes up to 6A. Does this mean I need a protection circuitry? Am I missing something?
Thanks in advance.