This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: PMP4311 schematic and BOM

Part Number: UCC28070

We are designing Interleave PFC with UCC28070 follow the ref. design PMP4311. 

We downloaded BOM and schematic from this link. http://www.ti.com/tool/pmp4311

But we found that the material value in schematic & BOM are different.

Example : =

C38, C39, C47,C48  : value in schematic is 4700pF but value in BOM is 1000pF. 

C66 : value in schematic is 220uF but value in BOM is 1000uF.

So, which one is the correct one ?  Should we follow value in schematic or value in BOM ?  or Does it have any new version of PMP4311 's schematic & BOM ? Thank you.