Hi,
I actually search some information about multiphase buck design and more particularly about input capacitors selection.
I find a report (SLTA055) which talk about input capacitors calculation. However, this article is only talking about monophase design.
So i found other reports such as slyt675, slyt 449 and more recenty slva882. However, Cin(min) formula for multiphase regulator are no more provide.
From normalized RMS input current calculation, i find total minimum capacitance needed for a 3-phase design. I think it's good but can you confirm the formula of Cin(min) ? My design is the same as shown on the Figure 1 from SLVA882.
Here is the formula i use:
Cin(min)=(Iout/(Vin p-p ripple * Fsw))*(D-(m/N))*(((m+1)/N)-D)
where:
Iout is the output load current
Vin p-p is the maximum allowed peak to peak ripple for input volage
Fsw is the switching frequency
D is the duty cycle (Vout/(Vin *efficiency))
m= floor (N*D)
N, number of phase
Then, here is my other question: is this Cin(min) calculated is available for only 1-phase or for all 3-phase regulators? I mean, I have to add the same number of capacitor for each phase or is it available for all 3-phase (I think this is the good solution)?
Thank you for your support.
Best Regards,
Mickaël