Hi,
In TPS53355 application example in datasheet, it is mentioned that Cout must be selected such that equation 14 is satisfied.
For 28A current, 12V input , 0.8V output, I got L = 320nH.
C1= 10nF, Fsw=250kHz, R7=6K ( to maintain equation 15 value less than 50mV)
N=2 , Ton= (Vin/Vout)*(1/Fsw)= 266.67nS.
D=0.8/12= 0.0667.
By substituting these values in equation 14,
Value of Left hand side of eqn=6.533E-07 for Cout = 100uF
Value of Right hand side of eqn = 2.66E-07
The equation satisfied ( left hand side value greater than right hand side value) for Cout=100uF, but the WEBENCH gives Cout as 2100uF.
Please let me know whether my calculation is correct.
Regards,
Madhu