Hi,
We are having an issue with our product using this battery IC. Somehow we get into a state were the output voltage is set to 1.1 V (below our CPU operating voltage) and our product seems bricked until we open it up and disconnect the battery to reset the BQ25120 and bring the SYS output back to the desired 1.8V. So we are wondering is there a fault or some event this part can experience which would cause the SYS output to drop to 1.1V?
We are never writing to the control register that would change the voltage from 1.8V so we are scratching our heads at this point. Any help would be appreciated.
Thanks,