This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40304: How is the value of RCS(R8) chosen

Part Number: TPS40304

Hi,

Can someone help me to understand why the value of 4.02Kohm is chosen instead of using the calculated value i.e. 7.1 Kohm?

Ref Page 21/39(SLUS964B) , the calculated value of RCS is 7.1Kohm which is R8 in Figure 18.

May I ask why in Figure 18, RCS(R8) is 4.02Kohm?

Why is this value chosen and how to get this value?

Thank you,

Angie