We are using TPS65150 LCD driver to drive display. We are using exactly same as application notes reference design.
It works fine with short distance between driver and LCD panel.
But one of new requirement is to increase the distance between the LCD panel and the driver by about 15cm long.
With this increase in length the driver getting very hot and display goes blank and all the o/p voltages drop to 0V.
Let us know is the long distance is over loading the driver. How to prevent getting hot and shutting down?