This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25892: BQ25892 is not charing while register readback is in fast charging

Part Number: BQ25892

Hi team,

My customer is using BQ25892 in their VR project and found that BQ25892 is not charging, then we readback the register and found the register status indicate the device in fast charging. please suggest if any mistake with schematic and register setting, if not, please suggest how to debug this issue, thanks. 

Kevin 

1. please help to review the schemaic and suggest if any issue .The input is from PC USB port. 

2. readback of register setting/status, please suggest if the setting is Ok.

root@avl7420:/ # cat sys/class/i2c-adapter/i2c-0/0-006b/registers             
Charger 1:
Reg[0x00] = 0x52
Reg[0x01] = 0x06
Reg[0x02] = 0x5d
Reg[0x03] = 0x16
Reg[0x04] = 0x8f
Reg[0x05] = 0x13
Reg[0x06] = 0x8e
Reg[0x07] = 0x8d
Reg[0x08] = 0x03
Reg[0x09] = 0x44
Reg[0x0a] = 0x73
Reg[0x0b] = 0x26
Reg[0x0c] = 0x05
Reg[0x0d] = 0x12
Reg[0x0e] = 0x39
Reg[0x0f] = 0x3b
Reg[0x10] = 0x6f
Reg[0x11] = 0x97
Reg[0x12] = 0x00
Reg[0x13] = 0x12
Reg[0x14] = 0x45

  • Kevin,

    The TS pin is reporting a COLD fault, meaning that the charger thinks the battery is too cold to safely charge.  How is the TS pin connected?  There should be a resistor divider from REGN and connection to battery thermistor.