This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: bq25703A / Efficiency result is too low

Part Number: BQ25703A

Hi,

I tried to simulate bq25703A Webench to see the light load efficiency, but it looks like the simulation does not include PFM mode. The Webench result show too low efficiency compared with the data in datasheet as attached. Please check it and discuss with MLC team.

webench_design_bq25703A Vin=5V Vout=8.4V Iout=0.1.pdf

Best Regards,

Satoshi / Japan Disty