This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Configuring for specific battery on bqstudio

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO, BQ76930EVM, TIDA-00792

Hi,

I am currently using the BQ76930EVM with the BQ76200EVM to manage the charging/discharging of our battery. I am using a battery with 6 cells, can hold 22.2 V, 20C discharge, and discharges at 16000 mAh and I was not sure on how to configure it on the bqstudio software. I was wondering if I could have some help on knowing what settings to change and to what? Thank you.