Hi team,
I am currently working with a design that has the following specs:
- Vin = 12V
- Vout = 6V
- Iout_max = 15A
Based on the datasheet, I have come to the conclusion that in order to follow the restraint of t_off > 725 ns, I require a switching frequency that is less than 690 kHz. With this in mind, I was able to calculate ET for varying switching frequencies, and determined that my inductor of choice would fall in the range of L43, L44, or L45 (depending upon the switching frequency I end up going with). The datasheet recommends the following inductors for this case:
- HA3778-AL from Coilcraft for a 1.5 uH solution
- B82477-G4102-M from EPCOS for a 1 uH solution
However, both of these are too tall for my design. Therefore, are there any recommendations for a shorter inductor that can still work for this design? I did some research myself and landed across the XAL7020. However, this is so small, I was worried it may have other negative effects that I am not considering.
Let me know if there are any other inductors that would fit this criteria, or whether the XAL7020 will work and I am just being to cautious.
Thanks!
Andy