This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: Enable Hybrid-mode failed

Part Number: BQ24780S

Hi Sir,

We send SMBus command to set the bit 2 of register address 0x37. After that, we detect the high level of TB_STAT and it seems that hybrid power boost mode is not working.

What is the condition to enable Hybrid mode?

1. Input current higher then current limit setting?

2. Set 0x37H[2] enable

3. From datasheet about BATPRES#: "The host can enable charging and hybrid power boost mode by write to REG0x14() and REG0x15() when BATPRES is HIGH" , so this means, I couldn't connect BATPRES# to ground if I want to enable hybrid mode?

4. Is there anything I need to notice?

Please help on this, thank you!!