This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659037: Total capacitive load per phase

Part Number: TPS659037
Other Parts Discussed in Thread: AM5718

Hi,

The TPS659037 Design Guide (SLIA088) section 2.2.2 states that "The total capacitive load per phase should not exceed 57μF, including decoupling capacitors at the load. Reduce the output capacitance to a minimum of 20 μF if required."

I've been looking at the AM571x Industrial Development Kit (IDK) where the TPS659037 PMIC is used together with an AM5718 Sitara MPU. Several of the SMPS outputs have loads above 100 μF. For example VSMPS3, which powers VDDS_DDR, has the following decoupling capacitors:

C278 = 47μF
C441 = 100 μF
C6 = 10 μF
and some smaller values caps...

Why isn't the Dev Kit following the recommendations? What are the consequences if any?

Regards
/F