This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5523: Driving external clock faster than 32.7KHz

Part Number: LP5523

Hi All,

I hope your week is going well.  I'm working with a system with several LP5523 chips tied to the same external clock for synchronization.

In section 6.10 of the datasheet, the specification shows a min/max high/low time for the external clock of 6us.  That translates to a maximum 83KHz operation.

Other than programs executing faster (subnote 5 in section 6.10), are there any other side effects or downsides I should be concerned about if I run the external clock at 80KHz?

Thanks for your time!

Tim Kutscha

Simplexity Product Development