This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95 Max Error Stuck at 5%



Hi

 

I am struggling to get a BQ20z95 based battery to update Qmax and the Ra table, it seems to be stuck with a MaxError at 5%.  I have cycled the battery with long pauses (more than 5 hours) at both the fully charged and fully discharged conditions, but MaxError stays at 5% (meaning that Ra table has updated prior to a Qmax update).

 

The battery configuration is 4S3P, 6.6Ah.  The profile is as follows:

1.       Charging it at a CC of 3A and CV of 16.8V until TCA

2.       Wait 2 hours

3.       Discharging at 3A until TDA.

4.       Wait 5 hours

 

I have also tried the following profile:

 

Neither of these profiles have worked, Max Error stays at 5%.

Is there a better profile I should be using to cycle the battery to achieve 1% MaxError?

Best regards

Steve Dodds

1.       Charging it at a CC of 3A and CV of 16.8V until TCA

2.       Wait 2 hours

3.       Discharging at 3A until for 30minutes.

4.   Repeat 2 until battery fully discharges

5.       Wait 5 hours 

  • The 5% indicates that Ra table updates have happened but Qmax updates have not. There are several issues that could causes this. It's hard to tell without a log file, but based on your profile, it looks like you are using too high a current in your learning cycle.  A Qmax update during learning requires 90% of Qmax to be discharged from the battery. If the current is too high or the taper doesn't get the battery full enough, it can be hard to meet the 90% requirement.

    Please follow these steps exactly with a new pack (IT hasn't been enabled yet):

    When no close Qmax value is known:

    1. Even though accurate capacity is unknown, set Qmax and design capacity to the cell capacity shown in the data sheet. Do not send IT enable command 0021.

    2. Send SMB command 46, word 0006 to turn on the FETs.

    3. Discharge the pack down to termination voltage at a C/5 rate.

    4. Let it relax for 5 hours or more.

    5. Send the IT enable command (0021). Bits QEN and VOK in Operation Status are set.

    6. Charge pack to full capacity until the taper current is reached and the FC bit is set.

    7. Let it relax for 2 hours. Qmax is learned at this point; this can be verified by MaxError changing to 3% and Update Status to 5.

    8. Discharge the pack down to terminate voltage at the typical low rate of your application. For laptops, it is usually C/5. The MaxError changes to 1%, and the Update Status changes to 6.

    9. Repeat steps 4 and 6 to 8 one more time to verify the gas-gauging accuracy.