This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: feets colsed on start-up, display button dont work

Part Number: BQ4050
Other Parts Discussed in Thread: BQSTUDIO

Hello! Need help again))  The device's scheme with bq4050 differs from the typical application in datashet in the following points:

1. 2-cell battery, so VC4-VC3-VC2 are shorted

2. No 2-nd level protection use, so FUSE pin is not connected (just in air, mb its thats the reason?)

3. PTCEN and PTC connected to Vss (GND)

4. I used IRF8788  FETs (instead Si7116DN)

5. Used 4 Mohm pull-up resistors on power FETs (but I think its even dont metter)

The problem is: device works well and connected to bqStudio, but FETs ARE CLOSED.. If I apply charger to the battery  bypassing FETS, cap. counter works well. Also I can calibrate termal sensors, surrent sensor and cell voltages. But I fets are closed. I can toggle LEDs by command from bq Studio, but display button and  command dont  do any result on LEDs even the cap. counter have 100% capacity.

Registers screenshot below.