This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22965-Q1: Maximum output capacitor value

Part Number: TPS22965-Q1


Hi,

We got a question from customer about TPS22965-Q1.
Could you help us?

[Question]
They are concerned about maximum output capacitor value. When the ouput capacitor is too big, they are thinking below concerns.

 - It will cause to generate of heat the IC at QOD event.
 - The IC can't control output voltage slew rate at start-up.

So they want to avoid these issue. They would like to know the recommended maximum output capacitor value, considering these issue. Could you give us your opinion?

 - Their condition -
 Vin=3.3V
 Vbias=3.3V

Best Regards,
tateo