Other Parts Discussed in Thread: BQ34Z100-G1, GASGAUGECHEM-SW, BQSTUDIO
GPC Support,
Attached is my submission to the GPC along with the report I received. It says that “Best chemical ID : 6100 Best chemical ID max. deviation, % : 100” and that “Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule”. I’m hoping to use these battery pack design (5 x FDK HR-DU cells in series) with the bq34z100-G1.
Should I proceed using the recommended chemical ID (6100) or is there a problem with my data that I should correct first? If I proceed with 6100 do you believe the gauge will function properly?
Thank you,
Paul.FDK HR-DU submission 7.zipFDK HR-DU submission 7-report.zip