This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM3150: low current

Part Number: LM3150

Tool/software: WEBENCH® Design Tools

Hello, I have made a power supply using LM3150.

My english is not that good.

The problem with the design is that it seems that the output current is severely limited.

The design was made for 8V and 5A  and the limit of the unit is actually around 1A.

I have used Webench.

Input Voltage : 14 ~ 24V

Output Voltage : 8V

Ouput Current Max. : 5A

Switching frequency : 440KHz

Ouput : 8V @ 0.5A (SW Pin)

Ouput : 8V @ 1.5A (SW Pin)

The only changes compared to the Webench BOM were:(Yellow)

Regard