Do you know what is the rated power of this stepper motor?
- i wish to drive it with a ti.com product
It is the 6V, 18.5 Ohms per winding (UBB1/5) type…….
http://www.auf-vertrieb.business.t-online.de/pdf/UBB.pdf
-the stepper has two windings.
Am I right in assuming that this stepper motor’s rated power is 2 * V^2/R = 3.89W ?
If the rated power is indeed this figure of 3.89W, is it ever permissible/adviseable to drive this stepper motor with a power higher than this rated value?
-If so , then for how long may I drive the stepper motor at a power level which is higher than the motors rated power level?