Other Parts Discussed in Thread: BQ24630
We have been using LM3478 to charge a LFP battery. We are using a micro-controller in our design ans hence not using dedicated battery charger to save cost and as micro-controller provides better management. We used Webench design to get the voltage output of 18.1 Volts and current limit of 1.2 Amps. The input voltage ranges from 10 Volts to 16 volts (Automotive nominal 12V range).
Schematics and PCB layout attached. The global label "Charge_Enable" is controlled (connected to GND) by a micro-controller.
Everything works fine in our circuit except the current limit. The circuit supplies as much current as the load wants without limiting the current.
What could be the issue? Do we need to use an external current limiter?