This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS55340: WEBENCH ISSUE

Part Number: TPS55340


Tool/software: WEBENCH® Design Tools

Hello,

Why is Webench not generating any solution for TPS55340 ?Is there anything wrong with WEBENCH ?

I was able to generate solutions 2 weeks ago. Now, in the past one week ,it does not seem to work.

I want to design a boost converter with this IC with the following spec.

Vin = 4 to 20V

Vout = 24V

Iout = 0.18A

I would really like to see the Webench designs for optimisations in the area required and efficiency.

Thanks,

Ajay