Dears,
When only use the Battery connect to the system, the BQ24250 can't working sometimes,I use multimeter to test the SYS and LDO pin's voltage, it's 0V; And If I plug the adapter to the Vin pin ,the BQ24250 can working normal, at this moment that I remove the adapter and the BQ24250 can recover work, I don't konw what's can cause the BQ4250 can occur the problem untime? It's like go into sysoff mode, but I don't to operation the register use code. Could you kindly give me some suggestion to solve the problem? Thanks a lot.
Best regards,
Jacking