This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2400: Does not send any signal

Part Number: EV2400
Other Parts Discussed in Thread: BQ78350, , BQSTUDIO

We have a EV2400 with firmware v018. It is connected to a board that has a bq78350 controller through the I2C port. We installed the EV2400_support_Components_20110524.

The device is detected by Windows. The three LEDs are on. We tried to communicate with it using the bq769X0 Evaluation Software but we got the "unable to detect a connected device" message.

We put an oscilloscope on the clock pin of the EV2400 and could not detect any signal when the Evaluation Software starts or when sending the Read Data command. It seems the EV2400 is not sending anything through the I2C port

We are running the app on a Windows 10 PC

Is there anyway to check if the EV2400 is working correctly?

Thanks