This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53679: About VOUT_COMMAND resister.

Part Number: TPS53679

Hi all,

I don't understand about VOUT_COMMAND resister.
What is it? please tell me the function.

The resister is set default(1.7V).
So I  tried changing the resister value by GUI, however I couldn't change the value.

I attached error message in the following.

10:26:16.475: TPS53679 @ 88d: VOUT_COMMAND [0x21,Rail #1]: wrote 1.720 V [0x007B] to the device and it was ACKed,
                       but a write verification read back returned 1.700 V [0x0079]

Best Regards,
Sho