This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61196: wanna make multi channel serial white flash light driver circuit of 24V demanding for μs class turnning on delay and 1μs-1s light on time, precisely controled flash current is up to 3A

Part Number: TPS61196


any suggestions?

  • Hi,

    The TPS61196 is not suitable for flash applications. if you could share some more details about your application we can direct you to the appropriate person to help you find a suitable device. I will close this thread, please open a new thread in this forum without a device part number attached.