Part Number: TLV62095EVM-840
Hi Support,
We have tested the TLV62095EVM-840 EVB, we change R1 from 200k to 82k ohm for 1.2V output.
Blue marker is our measurement result with 3.3V input, turns out we found that our result do not align with the red line shown in the datasheet, efficiency is around 8% lower at the our target loading (3A),
Could you advice if there are any way to further improve the efficiency?
Thanks.