This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54329: TPS54329 Loop stability

Part Number: TPS54329


Use TPS54329 to realize 12V to 3.3V 。Select  the C20   68 pF,   the phase margin of test is best.  But the datasheet of TPS54329 on Page 13  descripts  the capacitor is 5~22 pF。Can I choose  68 pF?

The Phase Margin Test Result   when  C20=68pF