Part Number: LM5116
I would like to use an LM5116 for a software controlled, variable output DC-DC, let's say 60 Vin and 35...55 Vout. My idea was to change the output voltage divider ratio by using a digital potentiometer, reed relays or similar technique. In your opinion, is this possibile and/or advisable? Many components have to be selected based on the output voltage, and while in some cases (e.g. input and output capacitors) is quite easy to determine the worst-case scenario and select a one-size-fit-all solution, in other cases this is more difficult to do:
Output inductor, ramp capacitor: selected based on the minimum output voltage?
Input capacitors, output capacitors, soft start capacitor, MOSFETs: selected based on the maximum output voltage?
Error amplifier compensation: ???
The other components (current sense resistor, bootstrap capacitor etc) do not seem directly related to Vout.
Am I doing something horribly wrong?
Thank you!
L.