This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EV2400: BQStudio will not recognize any part

Part Number: EV2400
Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50,I'm running windows 7 professional, 64bit. Certain USB ports will not install the drivers for the EV2400 (I get an error when I plug the device into the port, and cannot update or reinstall the driver from the device manager). Other ports will show that the EV2400 was successfully installed, but BQstudio will not recognize that it's connected, will not detect a fuel gauge, and will not interface with the fuel gauge if I manually tell it what fuel gauge is connected to it. I'm seeing this problem on multiple EV2400s and with multiple evaluation boards for the BQ40z50. Is there a link the EV2400 drivers so I can install them manually, rather than relying on the BQstudio software to do it for me?