Other Parts Discussed in Thread: BQ24600
Hi there,
I have recently ordered the bq24600EVM (HPA421) to evaluate. I performed the test listed on the User Guide successfully. I was able to do:
- AC ADAPTER DETECTION THRESHOLD Test
- CHARGER REGULATION VOLTAGE Test
- CHARGE CURRENT Test
When I switched my DC load with a LiPo battery I wasn't able to see any charge current. This test was done without a load on VSYS
- STAT: blinking
- CHGEN: on
- PG: on
VBAT was configured to 14.7V charge voltage by replacing R15 with 110Kohm resistor.
Questions:
- What can cause the charger not to recognize the presence of the battery ?
- The EVM BOM shows a 10mohm Rsense that defined the maximum charge current but the board is configured to allow only 3Amax. What's the actual value of Rsense (i will measure that later but if you could confirm that it'd be great)
Below is a picture of my setup.