Other Parts Discussed in Thread: UCC2808A-2Q1, UCC2808A-2
I'm using the UCC2808-2 in a push-pull topology 50% D.C . The chip powered by 9.5v power supply specified for it only . There is no voltage surges of any kind , and the chip drives 2 mosfet drivers so
there is no load on the outputs .It seems that in the history our engineers had failures on this chip and they add a series resistor of 20 ohm on it's VDD input mayabe because the thought that
there is a problem with the VDD power but i checked it and i didnt found any problem .I my self encounered some fails with this chip in the last months . The failure is that the outputs dosnt operate and
there is no oscilation on the RC and i measured the current through the VDD pin and its 5 mA .I checked the Data Sheet and so to my suprised that its recommended junction temp is 85 and
"junction=ambient " ???? .I want to know if its real data ( junction temp) or a mistake in data sheet ? . I think that the failure apeared in our design because of the high ambient temp (8 7 ambient )
I have another question , I saw that there is an automotive version of this chip that is UCC2808A-2Q1 and this chip is defined -40 to 125 ambient . I want to know what is the diffrent between them that
makes it more high temp resistant ?
Thanks