In my design, the TPS51200 seems to be operating normally, except PGOOD is always "low." I measure VO as 0.891V and REFOUT as 0.899V, well within 20% specified in the datasheet for the PGOOD signal to be asserted "high." I have a 10k pull-up connected from PGOOD to +3.3V. Is there another reason PGOOD might be "low" (other than an out-of-bounds output voltage)? For example, will PGOOD stay low if the output current is above some threshold (the datasheet does NOT indicate this is the case).