Other Parts Discussed in Thread: UCC28070
Hi everyone,
I am conducting a feasibility study on designing high power chargers with below specs,
3 phase 415V 50Hz input
110/220V DC output,
High efficiency >90%
The idea is to use a Front end interleaved PFC to generate intermediate 400VDC which shall be stepped down using Phase-shifted full bridge converter to 110/220V for batteries.
Some Challenges could be,
Finding high Current IGBTs.
Selecting an ideal switching frequency which may be limited to around 10kHz.
Designing Transformers(DC/DC)to handle high currents and with low leakage inductance to reduce ringing.
Designing Inductors to handle high currents(~400A).
Can UCC28070 and UCC28950 be used to achieve this.
Can anyone see any other significant challenges.
Any thoughts will be very much appreciated.
Thanks